SYSTIMAX® Solutions Donates High Performance Cabling to Levine Children’s Hospital

100 000 feet of SYSTIMAX® GigaSPEED® XL7 cable to connect new Charlotte hospital
28 novembre 2005 RICHARDSON, Texas

SYSTIMAX Solutions™, the worldwide leader in structured connectivity solutions, today announced that it plans to donate 100 000 feet of SYSTIMAX® GigaSPEED® XL Category 6 non-plenum data cable to Levine Children’s Hospital, part of Carolinas HealthCare System (CHS), being built in Charlotte, North Carolina. The donation is part of a community-wide effort to build a state-of-the-art pediatric medical center to serve the growing number of children in the Charlotte area, which is expected to increase by 23 percent over the next eight years.

“We already are operating at full capacity, so we knew we needed to build this hospital to plan for the future growth in the area,” said Betty Kuhn, senior director of development services for the Carolinas Healthcare Foundation, the charitable arm of CHS. “It also was important to build this hospital in the most financially efficient way possible, and that is why gifts like the one from SYSTIMAX Solutions are so crucial. The cabling they will provide for this project will last us well into the future.”

The total cost of the Levine Children’s Hospital project will be an estimated $85 million. Fundraising efforts and in-kind donations from CHS employees and executives, private donations and friends of the hospital, such as SYSTIMAX Solutions, are expected to raise $60 million of that amount.

“Of all enterprise applications for our product, hospital environments prove one of the most critical. Large digital medical files need to be able to be transferred in as little time as possible and require the cabling infrastructure to support that kind of bandwidth need,” said Peter Karlsson, senior vice president of sales for CommScope’s enterprise business. “We are more than happy to contribute to making the Levine Children’s Hospital dream a reality so that it can have the infrastructure to support its long-term needs.”

The SYSTIMAX GigaSPEED XL Solution combines the simplicity and versatility of copper cabling with support for the most demanding gigabit applications. With performance well beyond Category 6 specifications and transmissions almost three times quicker than Category 5e solutions, the GigaSPEED XL Solution gives desktop systems less downtime and more bandwidth-intensive throughput than ever before. It is an ideal choice for businesses whose applications require real-time data, fast file transfers and streaming media. In addition, its superior performance across a 250MHz frequency range offers potential for multi-gigabit throughput in the future.

Forty-one patents have been granted on innovations that help the GigaSPEED XL Solution achieve a breakthrough in Category 6/Class E copper cabling performance.

Today ~ The Children’s Hospital at Carolinas Medical Center

The Children’s Hospital at Carolinas Medical Center (CMC) treats an average of 130 children each day – more children than any other hospital in North Carolina. Located on the seventh floor of CMC, the current facility houses a 78-bed general pediatrics unit, a Level IV Neonatal Intensive Care Unit, a Neonatal Progressive Care Nursery, a Pediatric Intensive Care Unit, and a Children’s Specialty Center. Named by Child Magazine as one of the top 25 children’s hospitals in the country, the hospital serves as the regional referral center for certain pediatric transplants and pediatric surgical services.

Tomorrow ~ Levine Children’s Hospital

To accommodate projected growth of up to 95 000 children in this community during the next decade, CMC will open Levine Children’s Hospital – a 12-story, 234-bed facility designed with family-centered care as a top priority. The hospital will feature larger patient rooms to better meet the needs of children and their families, a new Family Resource Center with a pediatric health library and work stations, a 13-bed rehabilitation unit, and extensive child life program areas and resources.

Scheduled to open in 2007, Levine Children Hospital will be the third largest children’s facility in the Southeast and will offer several of the region’s “firsts,” such as the first day hospital, cardiac intensive care unit, and 24-hour pediatric emergency department.

About SYSTIMAX Solutions

SYSTIMAX Solutions™, a CommScope company (NYSE: CTV), is a worldwide leader in structured cabling systems and provides integrated end-to-end connectivity solutions for voice, data, video and building management applications in both wired and wireless enterprise networks.

SYSTIMAX Solutions supplies its high performance and market-leading range of products through a network of highly skilled BusinessPartners. The product range includes the copper based GigaSPEED® X10D and GigaSPEED XL Solutions, the fiber-optic LazrSPEED® and TeraSPEED™ Solutions and the intelligent patching iPatch® System. The SYSTIMAX AirSPEED™ Solution adds a wireless option to the portfolio. SYSTIMAX Labs and the people who have spearheaded these innovations will continue to play an integral role in the future success of SYSTIMAX Solutions. Currently the company’s BusinessPartners install an average of over 1 000 miles (1,600km) of SYSTIMAX cable every day in approximately 100 countries worldwide. For further information please visit http://www.systimax.com.

Forward-looking Statements

Ce communiqué de presse comprend des déclarations prévisionnelles basées sur des informations dont dispose actuellement la direction, des convictions de la direction, ainsi que sur un certain nombre d’hypothèses concernant les événements futurs. Les déclarations prévisionnelles ne constituent pas une garantie de performance et sont soumises à un certain nombre d’incertitudes et d’autres facteurs, ce qui pourrait entraîner des différences significatives entre les résultats réels et ceux actuellement attendus. For a more detailed description of the factors that could cause such a difference, please see CommScope’s filings with the Securities and Exchange Commission. En fournissant des déclarations prévisionnelles, la société n’a pas l’intention et n’assume aucune obligation ou devoir de mettre à jour ces déclarations à la suite de nouvelles informations, d’événements futurs ou autre.

Media Enquiries:
M/C/C for SYSTIMAX Solutions
Sadie McCrary Tel: 972-480-8383, ext. 222
sadie_mccrary@mccom.com
or
For Carolinas HealthCare System
Kirstin Ashford
Tél : 704-355-4048
kirstin.ashford@carolinas.org