Communiqués de presse

15 octobre 2019

Tessco et CommScope collaborent pour proposer des solutions sans fil de sécurité publique

TESSCO Technologies Incorporated (NASDAQ:TESS), a leading value-added distributor and solutions provider for the wireless industry, today announced it has secured the entire first year production capacity for CommScope’s new public safety product. CommScope’s Bi-Directional Amplifier addresses a key need for reliable, cost-effective public safety wireless systems. more

19_Tessco_logo

14 octobre 2019

CommScope Sues Rosenberger to Protect Trade Secrets

CommScope has filed a lawsuit in the United States District Court for the District of New Jersey against Rosenberger, several of Rosenberger’s legal entities and two former CommScope employees now employed by Rosenberger. more

ektron(2)

11 octobre 2019

CommScope to Acquire Base Station Antenna Technology from Fractus

CommScope, a global leader in wireless and wired technologies, has agreed to a technology transfer agreement as a result of a settlement with Fractus S.A., a Spanish company that developed key antenna technology for use in wireless base station antennas. more

ektron(2)

8 octobre 2019

Foxtel sélectionne CommScope pour redéfinir le visionnage de la télévision en Australie

CommScope today announced its continued partnership with Foxtel, Australia’s leading Pay TV operator, to bring The New Foxtel Experience to subscribers across the country. more

19_Foxtel_Ektron

3 octobre 2019

CommScope Roadshow Dives Deep into the Forces Transforming the Data Center Industry

CommScope, a global leader in infrastructure solutions for communications networks, will host a six-city tour to educate data center professionals on how 5G, next-generation speeds, new physical layer topologies and other trends are transforming the data center industry. The Data Center FiberCon roadshow – which will center on the theme “The Power of Progress” – will feature content by data center infrastructure, planning and architecture experts from CommScope and other more

19_DC_Fiber_Con_Ektron

24 septembre 2019

CommScope apporte un choix et un contrôle sans précédent aux créateurs de réseaux à large bande ; révélant des gains spectaculaires en termes d’échelle et de latence plus faible

Poursuivant son leadership au profit des technologies réseau nouvelle génération, CommScope a aujourd’hui annoncé les trois nouveaux piliers qui ont permis d’améliorer l’échelle, la vitesse et la latence. The advances – in architecture design, interface speed, and edge performance – create unprecedented choice and control for broadband network operators. All will become elements of the company’s Distributed Access Architecture (DAA) and 10G portfolios. CommScope will discuss and demonstrate the new technologies at the SCTE•ISBE Cable-Tec Expo beginning more

19_SCTE_2019_10G_ektron

24 septembre 2019

First Field Test Begins for Japan’s Next-Generation Wi-Fi Standard IEEE 802.11ax (Wi-Fi 6®)

TOKYO, JAPAN, 25 September, 2019— Ruckus Networks (now part of CommScope via acquisition) and Wire and Wireless Co., Ltd. (Wi2) today announced that they have started the first field tests1 of t more

16 septembre 2019

RUCKUS NETWORKS R750 ACCESS POINT NOW Wi-Fi CERTIFIED 6

Ruckus Networks (now part of CommScope via acquisition) today announced that the R750 802.11ax indoor Wi-Fi® access point (AP) for ultra-dense client environments is Wi-Fi CERTIFIED 6™ from the Wi-Fi Alliance. This certification further validates the applicability of the R750 in ultra-dense client environments such as stadiums, hotels, convention centers and schools. Wi-Fi CERTIFIED 6 increases client device speeds by nearly four times that of Wi-Fi 5, optimizes network capacity, more

19_Ruckus_R750_Access_Point_Ektron

16 septembre 2019

FCC Approves CommScope CBRS Spectrum Access System for Initial Commercial Deployment

CommScope received official notification from the Federal Communication Commission (FCC) that its spectrum access system (SAS) to support the Citizens Broadband Radio Service (CBRS) is now certified for initial commercial deployment. With the notification earlier this year from the Institute for Telecommunication Sciences that its Environmental Sensing Capability (ESC) sensor passed testing, and the addition of Ruckus Networks’ Band 48 CBRS devices (or access points) and cloud services, CommScope is more

ektron(2)

15 septembre 2019

CommScope annonce des plateformes Smart Media Device et clients IP Wi-Fi6®

CommScope a annoncé aujourd’hui deux nouveaux venus nouvelle génération au sein de son portefeuille d’accélérateurs vidéo RDK : a Smart Media Device (SMD) platform 7852 featuring Wi-Fi 6® connectivity, as well as an IP Client VIP7802 with Wi-Fi 6®. Both devices include AOMedia Video 1 (AV1) and high dynamic range (HDR) capabilities. more

19_RDX_IBC_ektron